Items tagged with 计算机辅助制造 (CAM)
Bringing a robot bartender to market 2.5 times faster by eliminating design inconsistencies and streamlining development
CHALLENGES Design and prototype a fully autonomous robotic bartender called Yanu Eliminate design inconsistencies between designers and engineers KEYS TO SUCCESS Use a single platform for product development data Balance robotic innovation and function…
Addressing complexity with digital transformation
See how Wingcopter, Burgener, Yanu, Fiamma and eNovates are using Solid Edge to shape the future and transform their approach to product development.
优化产品设计实现轻量化
优化产品设计 当今市场瞬息万变,轻量化设计至关重要。也许不仅有特定的设计目标和限制,同时还需要以最少的材料用量设计出更轻的组件。 此网络研讨会讲解的内容: 如何创建更轻的组件 减少下游制造中的材料浪费 创建适于铸造或高分辨率 3D 打印的高度定制设计 相关资料: 获取 Solid Edge 免费试用版
Design Smart, Connected Products: ECAD-MCAD Collaboration for Better Harness Design
How to thrive as an engineer in an electromechanical world. Better Harness Design Engineers are being asked to work outside their normal domain with mechanical engineers often dealing with electrical requirements, and vice-versa. Electrical systems are…
2D 嵌套的价值
2D 嵌套过程是指在一个切削平面上安排 2D 形状,目的是生产尽可能多的产品而又尽可能减少浪费。使用现代化嵌套算法优化的嵌套样式,减少预制时间、废料和成本。本电子书将探讨 2D 嵌套的自动化如何能够改进工作效率、生产率和盈亏底线。 2D 嵌套的价值 无论您是制作皮革制品还是钣金,生产鞋子还是造船,2D 嵌套都可以帮助改进质量并节省时间和资金。这种高效性可以助推您的业务命脉并直接关联盈亏底线,具体途径包括:增加订单、减少原材料开支并提高生产效率。 本电子书将讲解 2D 嵌套的价值、如何节省时间和资金、…
Optimize your product design for lightweighting
Get your product designs into shape. Optimize your product design Design for lightweighting is critical in today’s fast-changing marketplace. You have specific design goals and constraints while needing to design lighter components with minimal materia…
借助高级加工技术加速数控加工
如何在不牺牲安全性或控制性的情况下加速数控加工?高级加工技术可以帮助加快加工并缩短收益时间。 数控加工之高级加工技术 时间对于所有车间而言都是最为重要的。越快完工,就能获得越高的收入。对于数控编程人员而言,这不仅意味着要迅速生成刀轨,而且意味着生成的刀轨要迅速运行。车间最终的利润是由生产的工件数量决定的。但是,过多的订单以及无法完成订单或满足客户要求,会对公司的信誉产生长期损害。车间确保利润的唯一方式就是,紧凑排班、保证工作质量并按时推进各项工作。 这种直接的车间盈利方式让数控编程人员压力倍增,亟需…
The value of 2D nesting
The process of 2D nesting is the organization of 2D shapes on a single cutting plane with the goal of producing as much product with as little waste as possible. The optimized nesting patterns, created using a modern nesting algorithm, reduce preparati…
How to increase speed and improve quality of part manufacturing simultaneously
You will learn solid tips and techniques for major improvements in part manufacturing Automate part manufacturing Automated solutions that integrate front-office functions such as design and CAM with shop floor operations were once reserved for large i…
Accelerate CNC machining with advanced machining techniques
How do you accelerate CNC machining without sacrificing safety or control? Advanced machining techniques can help speed machining and reduce time-to-revenue. CNC Machining Advanced Machining Techniques Time is of the utmost importance for machine shops…
Design a F1 Racecar Model
Follow this in-depth Solid Edge CAD tutorial design a sleek and stylish F1 Race car model.
Technology helps revive a classic name in timekeeping
Solid Edge helps revive a classic name in watchmaking After a watchmaking apprenticeship in Munich, Christine Hutter held various jobs with renowned watchmakers and jewelers in Switzerland as well as in Munich and Glashuette, Germany. Hutter wanted to…
Design a F1 Racecar Model
Follow this in-depth Solid Edge CAD tutorial design a sleek and stylish F1 Race car model.
2D Nesting in Solid Edge
Solid Edge 2D Nesting utilizes the most advanced and efficient nesting engine to generate best-in-class layouts optimized for two-dimensional cutting.
EIGSA reduces engineering development time by 60%
Equipos Industriales del Golfo, S.A. (EIGSA) is a Mexican company dedicated to the design, manufacture, maintenance and installation of pressure vessels, heat exchangers, air coolers and gas separators. The company was founded in 1988, focusing primari…